Part Number: TMS320F2812
Dear team:
When I use memcpy() function in F2812, I have included "string.h". The program does not prompt an error when compiling, but it will enter the illegal interrupt “interrupt void ILLEGAL_ISR(void)” as long as it runs to the memcpy() function after power on.
I transfer the initialization flash function from flash CD 3ee815 address to RAM through memcpy() function, and the running start address is 3f9915. After compiling, the MAP file is as follows:
FLASH_SET_FUNCS
* 0 003ee815 00000017 RUN ADDR = 003f9915
003ee815 00000017 DSP281x_SysCtrl.obj (FLASH_SET_FUNCS)
I checked that the assembly statement on 3ee815 address was correct, but after it was moved to ram, the assembly statement was confused. Check the address does not overlap, then what is the cause of this error?
Best Regards