This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Function call failed when add more variables in main.c files

Part Number: TMS320F28377S

Hi Expert,

There's an issue customer meets that adding more variables and used in main.c file, the main function could not be executed. And there's no error or warning after build the project.

We try the below ways to debug this issue,

  • disable the watchdog in .asm file, it's useless.
  • move and define the variables into other .c & .h file, the issue disappears.

Their project is based on CCS 6.0, TI v6.4.4 compiler version.

Could you please help to provide some debug methods about this case? Thanks!

Best Regards

Rayna