This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXDOCK28346-168 Documentation for new (USB-)Baseboard?

Hello,

today I get my ordered "TMDXDOCK28346-168" and for my surprise the "Dockingstation" is changed from the last one ordered last year!

It has the same purchase order number and on the order page is also nothing mentioned. (still the old picture & there is a notice which says "you will need an jtag-emulator")

Now it looks like there is also the usb-jtag device on board. (and to save some cent the Supply- & Gnd - headers are not populated)

So my question is now what have I to do, if I want to use my own JTAG-Device (JTAGJet).

How could I disable the build in one. I think I didn't can run both in parallel.

Also an annoying thing is that on J7 & J11 all Pins are labled GPIO-9. (but I hope that they are the same as on the old board)

Is there a documentation available for this new dockingstation (called DIMM168 USB EXPERIMENTERS BOARD)

In the BaslineSw (sprc675) only the old one mentioned.

 

Thanks,

  Stefan