My customer wants to understand the details about the phase shedding control in TIDA-1007. Could you please help check the below questions?
1) Did we implement the phase shedding and adding control during the zero crossing point? If so, if the load changes from light load to high load, how can it support fast transient response if it needs to wait for the zero crossing point?
2) Does it need to adjust the duty cycle during the phase shedding or adding? For example, if we change from 1 PH to 2 PHs, do we use the same duty cycle from the current loop for the both phases?
Thank you.