This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28388D: Ethercat as ethernet

Part Number: TMS320F28388D

Tool/software: Code Composer Studio

Is it possible to use the Ethercat connection as an ethernet connection.
I have an old code where I have all the communication set up with the ethernet, and I just realized, with the new board, F28388D, the shared RAM memory between the CM and CPU1 is way to small.

I then saw that the ethercat connection was connected directly to CPU1. Could that be possible to do that?

I have a DUT where C28 reads data from, then it stored in a ring buffer where i use the shared RAM. Then the CM core reads the data from the ring buffer and sends it to LabVIEW with an ehternet connection.

Hope you understand.

Regards 

Asbjørn Schram Anneberg