This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.





As David said the ADC result registers are read only, so the Simulink tools won't be able to inject your constant value that way. For the purpose of debugging your system, I think you could just re-map where the results are fetched to match the memory where you've placed your constant(or other data).
I suppose another method would be to abstract your control calculations externally to the PIL block and feed the values in there.
In either case you could still set up the ADC as it would be your system, just to have the ADC Interrupts/EOCs for triggering/timing reasons.
Best,
Matthew
Hi David and Matthew ,
Thank you for your answers and helps. Actually I want to mention about my problem more general.
I want to make PIL implementation using Matlab C2000 embedded coder
I successfully read EPWM value duty cycle(cmpa and time counter value ) according to this value I generated PWM on simulation beside on the Launchpad pin using EPWM . No problem here.
But I realized that there is no any input of the ADC block . According to PIL application voltage is getting from the voltage divider of plant circuit like a buck converter etc. But ADC block only accept the value via pin of the launchpad or microcontrollers.
For this reason I didn’t get the voltage value from the voltage divider circuit and insert it to ADC block. I want to implement this condition . I don’t want modeling a ADC block using matlab blocks , I want to use C2000 ADC block in order to analyze as if real value getting from voltage divider and adc makes sample,hold,quantization processes like a real application.
This is successfully done by PLECS like following figures;
You could see the simulation values(sensed values) enter the ADC block.
The inside of the adc block as follows;
This is an ADC type the way i want it to use my matlab PIL application(processor in the loop) . But as I mentioned above
The ADC block does not have no inputs in MATLAB like an ADC block have inputs as in the PLECS.
I don’t want to use PLECS because of the PIL modeling and out file creating difficulties(need to design some codes using code composer studio)
Compared to PLECS, Matlab out file generation and interface more simpler.
1-Do you have any works on this topic on your side((texas ınstruments )?
2-Are there any methods you can suggest?(I know you suggested some methods , but again I ask to you , you maybe give more general informations about this)
3- Will there be an improvement in this issue in the matlab c2000 embedded coder infrastructure in the coming years?
Thanks in Advance .
I'm going to ask someone to comment from the MW team; they should know the constraints/capabilities of the PIL blocks more completely than I do.
Best,
Matthew
Hi,
Our blocks that are shipped with C2000 support package are code-gen only. You cannot simulate these blocks to behave like a ADC peripheral.
Our ADC blocks always read the digital value as converted by the ADC peripheral of the MCU. So you need to code-gen to get these blocks to work either through external mode or as standalone.
We do have a project called SoC blockset that ship simulation ADC blocks.

But you need a separate license for the same.
You can also explore the use of variants to switch between codegen and simulation.
One of our Motor control blockset shipping example as this option. You can refer the same.
mcb_pmsm_foc_f28379d_dyno

HTH