Part Number: F28M36P63C2
Tool/software: TI C/C++ Compiler
Hallo,
We are using F28M36 P63C2ZWTT YFF-82ADFOW on our PCBs to control the joints of the robots. The chip is also running at a very high temperature, about 67 degree measured on the chip surface. The chip stops working in less than 1 minute without heatsink and could work 2 minutes with a 10mm*14mm*6mm ( W*L*H) heat sink on it. We try 14 and the 14 are all more or less the same. But before we use F28M36 P63C2ZWTT YFF-82APZEW. (The schematic, the layout, the PCB material and the factory stays the same.) The chips with this number is working well, but still with a high temperature 67 degree.
We use TMS320C28X Optimizing C/C++ complier V18.1.0.LTS. and code composer studio as IDE.
Can anyone help me why the MCU is always so hot ?
Why F28M36 P63C2ZWTT YFF-82ADFOW could not work with the same high temperature, but F28M36 P63C2ZWTT YFF-82APZEW can.
If anything more is needed, please just let me know.
Thanks a lot!
Xiyao Zhao