Part Number: TMS320F28069M
Other Parts Discussed in Thread: MOTORWARE, TMS320F28069, TMS320F280049C, C2000WARE, INSTASPINUNIVERSALGUI
Code Composer Studio is up to version 10.0 now. The INSTASPIN Universal GUI requires an old 6.0 version. I have encountered numerous links prodding me to use the 'Cloud' based GUI Composer v2 and I would rather not install the older CCS 6.x version if I don't have to.
I thought I would try it out. In the gallery I did find an Insta-SPIN project designed for another board / CPU. I figure that existing effort would save me time building the UI. However, after importing that project into GUI Composer v2, going to Project Properties, there is no TMS320F28069M device listed (only the non-M version). Does that matter for the GUI? Is this GUI Composer v2 suppose to work with the older motorware stuff?
I even tried selecting the TMS320F28069 (non-M) so see if the console would connect and it says 'Failed to connect to device TMS320F280049C.' - that isn't even the device I selected.