Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Dear TI Team,
Is there a sample program for core1 and 2 in TMS320F28379D which demonstrates the flash programming (for standalone application) with Interprocessor communication (IPC)?
I have gone through sample projects Lab4_cpu01 and Lab4_cpu02 provided in one day workshop at the following link.
https://training.ti.com/c2000-f2837xd-microcontroller-workshop
and it was useful to study the IPS instructions.
When I changed sample codes from "load and run from RAM" of Lab4_cpu01 and Lab4_cpu02 as per expected during when emulator is connected.
But whenever I do a power cycle (replugging the USB), IPCs are not functioning (evident from the status over LED).
I have attached cmd files for both the cores. There is no change in Lab4_cpu01 and Lab4_cpu02 main files. May I get some information to make them ( Lab4_cpu01 and Lab4_cpu02 ) working in standalone mode?
Regards,
Rupesh