Part Number: TIDM-BLPFC
Tool/software: Code Composer Studio
I have ordered the device from Texas Instrument i.e. TIDM-BLPFC i.e. using C2000 MCU with exactly F28035 Piccolo-A. Now as this controller is a reprogramable so I want to connect it with the simulink and CCS for debugging but it is having the problem:
When i want to debug this C2000 controller with CCS, when I use the laptop from my friend with windows 7 for debugging then the code is transferred successfully to the target. But when I use my laptop with windows 10 then I find a problem in the debugging. The target gets connects to my laptop but I can't transfer my program to it. It shows the following message i.e.
Break at address "0x3ff599" with no debug information available, or outside of program code.
So I want to know exactly where the problem is? Is it problem to program the C2000 with windows 10?
Regards
Khalid Javed
PhD Researcher at Ghent University Belgium.