This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F28379D: CPU1 does not gets debug but CPU2 gets debug

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

I had purchased new LAUNCHXL-F28379D. In that CPU1 does not gets debug and following error occurs as shown in following figure and gets exit.

 

I tried to debug on CPU2 and it gets uploaded and it had given the output correct. I also tried connecting CPU1 target and rest it. But still same error occurs. I had also tried different programs but same error occurs at CPU1. Is there any solution for CPU1 not working ? 

  • Akshay,

    It happens when the Device Variant is not selected correctly or compiler is not selected correctly. Can you try C2000ware DriverLib example?

    Looks like you are using CCS7. It is recommended to use latest CCS (10.1).