Part Number: TMS320F28388D
Hello,
I am trying to implement RAM test for CPU1TOCPU2MSGRAM and CPU2TOCPU1MSGRAM as a part of Powerup test. We write a specific pattern value into whole MSGRAM area and then read it back. If all the values are read back successfully, then the RAM test is passed, else the test is failed.
However, In our application, we use only a small area of MSGRAM for inter processor communication purpose and rest of the area is unused. So, I have few questions related to this RAM test.
Is it Ok to perform the RAM test only for the used memory bytes and skip RAM test for the unused bytes of MSGRAM? What is the recommendation from TI for the RAM test from Safety point of view?
If there is a single byte of MSGRAM that has failed RAM test and all other bytes passed the RAM test, does this mean, entire MSGRAM cannot be trusted?
Does TI has any Safety Manual/Guidelines for the use of TMS320F28388D in Safety related applications? If yes, please provide the document for the same.
Best Regards
Amulrass V