This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Digital Power, can't use 2P2Z function

Other Parts Discussed in Thread: C2000WARE

Hello. 

I am trying to make the Digital Power 2P2Z function work with the F28069 device but it is not doing anything I think. I have followed the instructions in the DPlib document. Everything builds and compiles without issues. I have defined an "Out = IQ24(0.0)" according to the picture below and I expect "Out" to change value as the program runs through "CNTL_2P2Z 1", but my "Out" is never changing from 0. 

As I run the program in debug mode I put a breakpoint at "CNTL_2P2Z 1" in my DPL-ISR.asm file, see picture below. But as the program passes my breakpoint my variable "Out" is not changing. I have set my 2P2Z coefficients such that I expect the number to change from 0 to something else. But no calculation is taking place I think.

What could possibly be causing this?

BR