Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
I want to use the serial com port capability of the FTDI 2232 device found on the docking station, specifically the slave UART. (Ideally I would like both the JTAG AND slave UART features.)
At present the ports appear as other devices in dev manager.
I have the device drivers on my system, C:\ti\c2000\C2000Ware_3_02_00_00\utilities\windows_drivers
There are a few...
I presume usb_dev_serial is the one I need? Please answer.
The process for installing needs clarification.
I can try to Update the drivers manually but all this does is enable the TI devices to be enumerated properly, one or other or both do not appear as comm ports.
How can I get the docking station to expose one or both of the com ports please?
Many thanks