Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: TEST2, C2000WARE, TMS320F28377D
I have an application which is a slightly modified version of can_ex10_mask (switch to CANB since that's what's on the dev board, changed the extended ID to match my CAN bus traffic and added some printf's) that works when I run it from RAM but it never indicates receiving a CAN message when run from flash. Neither the mbox bit in NDAT_21 nor the RXOK bit in ES gets set when running from flash.
I assume something isn't right with linker script but I can't figure out what the issue is. I've tried moving the .cinit section to FLASHF from FLASHB as FLASHB isn't big enough if you use printf's in the app. (Getting rid of the printf's and using the stock linker script doesn't make the app work.)
I've included (hopefully!) my main.c and I'm currently using the stock can_ex10_mask/2837xD_FLASH_lnk_cpu1.cmd linker script.
Any ideas on how to track down what I'm doing wrong?
#include <stdio.h>
#include "driverlib.h"
#include "device.h"
//
// Defines
//
#define MSG_DATA_LENGTH 8 // "Don't care" for a Receive mailbox
#define RX_MSG_OBJ_ID 1 // Use mailbox 1
//
// Globals
//
uint16_t rxMsgData[8]; // Buffer for received data
volatile uint16_t X, Y, Dim;
#define LED_SET_WARM_PWM 0x08280000
#define LED_SET_COOL_PWM 0x08280001
#define LED_SET_RED_PWM 0x08280002
#define LED_SET_GREEN_PWM 0x08280003
#define LED_SET_BLUE_PWM 0x08280004
/**
* hello.c
*/
int main(void)
{
int i;
uint16_t warm, cool, red, green, blue;
//
// If running from flash copy RAM only functions to RAM
//
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif
//
// Initialize device clock and peripherals
//
Device_init();
//
// Initialize GPIO
//
Device_initGPIO();
//printf("CAN Bus test: DEVICE_SYSCLK_FREQ = %ld\n", DEVICE_SYSCLK_FREQ);
//
// Configure GPIO pins for CANTX/CANRX
//
/* GPIO_setPinConfig(DEVICE_GPIO_CFG_CANRXA); */
/* GPIO_setPinConfig(DEVICE_GPIO_CFG_CANTXA); */
GPIO_setPinConfig(GPIO_12_CANTXB);
GPIO_setPinConfig(GPIO_17_CANRXB);
//
// Initialize the CAN controller
//
CAN_initModule(CANB_BASE);
//
// Set up the CAN bus bit rate to 500kbps for each module
// Refer to the Driver Library User Guide for information on how to set
// tighter timing control. Additionally, consult the device data sheet
// for more information about the CAN module clocking.
//
CAN_setBitRate(CANB_BASE, DEVICE_SYSCLK_FREQ, 1000000, 10);
//CAN_setBitTiming(CANB_BASE, 5, 1, 7, 4, 2);
//
// Initialize the receive message object used for receiving CAN messages.
// Possible flags: CAN_MSG_OBJ_NO_FLAGS, CAN_MSG_OBJ_USE_EXT_FILTER,
// CAN_MSG_OBJ_USE_DIR_FILTER
// Message Object Parameters:
// CAN Module: A
// Message Object ID Number: 1
// Message Identifier: 0x1F9FFFFA
// Message Frame: Extended
// Message Type: Receive
// Message ID Mask: 0x1F000000
// Message Object Flags: UMask, MXtd, MDir
// Message Object flag CAN_MSG_OBJ_USE_ID_FILTER enables usage
// of msgIDMask parameter for Message Identifier based filtering
// Message Data Length: "Don't care" for a Receive mailbox
CAN_setupMessageObject(CANB_BASE, RX_MSG_OBJ_ID, 0x1555aab4,
CAN_MSG_FRAME_EXT, CAN_MSG_OBJ_TYPE_RX,
0x1555aab4, CAN_MSG_OBJ_NO_FLAGS,
MSG_DATA_LENGTH);
//
// Start CAN module A operations
//
CAN_startModule(CANB_BASE);
//printf("CANB started\n");
//
// Start reception - Just wait for data from another node
//
while (1) {
//
// Poll bit0 in CAN_NDAT_21 register to check completion of Reception
//
//if(((HWREGH(CANB_BASE + CAN_O_ES) & CAN_ES_RXOK)) == CAN_ES_RXOK) {
if ((HWREG_BP(CANB_BASE + CAN_O_NDAT_21) & (1 << (RX_MSG_OBJ_ID - 1))) != 0) {
//
// Get the received message
//
asm(" NOP");
CAN_readMessage(CANB_BASE, RX_MSG_OBJ_ID, rxMsgData);
X = (rxMsgData[0] << 8) + rxMsgData[1];
Y = (rxMsgData[2] << 8) + rxMsgData[3];
Dim = (rxMsgData[4] << 8) + rxMsgData[5];
/* for (i = 0 ; i < MSG_DATA_LENGTH ; i++) */
/* printf("[%d]: 0x%04x\n", i, rxMsgData[i]); */
//printf("%u: %u, %u, %u\n", rxMsgData[6], X, Y, Dim);
#if 0
xy_to_tdrgb(X / 65535.0f, Y / 65535.0f, Dim / 65535.0f,
&warm, &cool, &red, &green, &blue);
printf("( => (%5u, %5u, %5u, %5u, %5u)\n",
warm, cool, red, green, blue);
#if 0
SendLED(fixture->fd, LED_SET_WARM_PWM, warm);
SendLED(fixture->fd, LED_SET_COOL_PWM, cool);
SendLED(fixture->fd, LED_SET_RED_PWM, red);
SendLED(fixture->fd, LED_SET_GREEN_PWM, green);
SendLED(fixture->fd, LED_SET_BLUE_PWM, blue);
#endif
#endif
}
}
return 0;
}