Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi team,
I have a problem with serial flash programming. I am trying to use your demo c2000\C2000Ware_3_03_00_00\utilities\flash_programmers\serial_flash_programmer.
I had set up the device as it is denoted on application note SPRABV4C (Serial Flash Programming of C2000™ Microcontrollers) and I was trying to download the kernel to F28379D CPU1 through USB-UART converter.
The PC application sends just one data frame and stop transmission and CPU don't respond. Always send the same byte, 0x41h and after that nothing happen. I checked two MCUs and I am sure that UART RxD and TxD have a direct connection to proper pins (GPIO28 and GPIO29). Both didn't respond to PC. Am I doing something wrong? Should I download the kernel to memory before bootload program via SCI?
Thank for help,
Best,
Mateusz Stasiak