This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO-C2000: CCS10 with C2000Ware 3.03 doesn't exit cleanly

Part Number: CCSTUDIO-C2000


Tool/software: Code Composer Studio

CCS updated C200Ware to version 3.03 the other day. Now every time I exit CCS, I get the following warning dialog:

  • Mike,

    Are you using it on Mac or Linux platform?

    I just tried on MacBook. I imported Led DriverLib example for F280049C. It works fine without any issue, it exits cleanly. 

    Can you try to create a new workspace, and then import any example, and check if it is working for you?

  • I'm running on an iMac. And of course, when CCS quits to switch to the new workspace, it doesn't complain about the NULL reference. Exiting from the new workspace and no complaint. Restart and back to my original workspace, exit, and no complaint.

    I did exit from my "workspace-v10" several time over a couple of days and got the message each time before opening the support ticket! And so as soon as I do file a support ticket, it magically fixes itself! Argh! I hate things that magically fix themselves!

    Oh well! Guess I'll close this one. Until it comes back just as magically!