Part Number: DRV8302-HC-C2-KIT
Other Parts Discussed in Thread: CONTROLSUITE
To whom it may concern
In DRV8302-C2-kit allocation and F28035 mux map, the hall inputs connect the GPIO40~42. And that ports have no eCAP in F28035. eCAP ports are GPIO 5, 19 ,24. That ports are allocated other things. So, I wonder how to use eCAP port, if want. The signal has 5V and if the port may not support 5 to 3.3 in the inverter circuit, it is impossible to me. Also, for your understanding, I attach the relative picture. Thanks for help and looking forward to your response.