Part Number: TMS320F28379S
Tool/software: Code Composer Studio
Hi ti experts,
i am using tms320f28379s to develop motor control board, ccs version is: v7.4.0.
an abnormal thing is found:
gpio9 and gpio22 are used to control two led lights
my question is: when motor runs on current close loop and let led flash with 1seconds interval, i can hear there is noise come out from motor.
but if stop led, the noise disappeared.
i am confused with this issue. the two gpio9 and gpio22 are only connected to control two led, i have no ideal why it is related to motor control.
pls help give some advice. thanks very much.
Feng