Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Hi,
Is this possible to write on EEPROM emulation flash sector every 5sec once while code is running from flash memory? when I am referring " e2e.ti.com/.../319481" thread in that mentioned "Note that on F2808, you cannot erase or write to the flash while executing code from flash. It is also typically very difficult if not impossible to keep your main application running in realtime when operating on the flash since the flash APIs are not interruptible.
Thanks&Regards,
Rani