Hello,
In case of an ITRAP, if illegal instruction flags are not cleared is the NMIWD counting like other NMIs or no WD and no reset in case of ITRAP?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
In case of an ITRAP, if illegal instruction flags are not cleared is the NMIWD counting like other NMIs or no WD and no reset in case of ITRAP?
Thanks.
Hi Dvir,
ITRAP does not trigger NMI so NMIWD counter will not count and no reset. It's another fault which user should have handler for.
Regards,
Vivek Singh
Hi Vivek,
Thank you for the prompt response.
But just to be sure, ITRAP does trigger a different kind of non-maskable interrupt, right?
As mentioned in SPRUHM8H:
"Illegal Instruction Trap (ITRAP)
If the CPU tries to execute an illegal instruction, it generates a special interrupt called an illegal instruction
trap (ITRAP). This interrupt is non-maskable and has its own vector in the PIE vector table. For more
information about ITRAPs, see the Illegal-Instruction Trap section of the TMS320C28x DSP CPU and
Instruction Set Reference Guide (SPRU430)."
Is this enabled by the boot ROM similarly to the NMI module?
Regards,
Dvir
Hi Dvir,
But just to be sure, ITRAP does trigger a different kind of non-maskable interrupt, right?
Yes, it's a different type of fault which can not be disable.
Is this enabled by the boot ROM similarly to the NMI module?
No, there is no SW configuration bit to enable/disable this.
Regards,
Vivek Singh