Part Number: TMDSHVRESLLCKIT
Hi,
My customers evaluate TMDSHVRESLLCKIT. They have two problems and please tell me about them.
Question 1:
They look at HVLLC-QSG[R3] and evaluate EVM.
They are looking at the Hardware Setup steps. And even if 390V is supplied, the power is not supplied in the controlCARD. (Probably U1 overcurrent detection is working.)
When they supplied 350V there, they was able to connect to PC (GUI tool).
Also, if you gradually increase it from 350V to 390V, it will work without problems even at 390V.
Is this usage correct?
Question 2:
I want to rewrite the program in the above situation. When connected to CCS, they get the following error message and can't debug.
C28xx: Error connecting to the target: (Error -1135 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Release 5.0.333.0)
Would you tell me how to rewrite the program?
CCS v4.1
TMDSHVRESLLCKIT
Best regards, Rei