This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AC Induction 3PH example on 28335

Dear Mr. or Mrs.


We want to use already made TI example of AC induction 3PH  (V/F) for 28335.

 

There are two options:

1. example sprc130 is for 281x family. The problem is that if we want to use it for 28335 then we have to change quite a lot of things to achieve that!

2. to use control suite in CCS4.

 

We've bought CCS3.3.

 

We are sure that someone has already made example of AC induction 3PH on 28335 for CCS 3.3.

 

Please be so kind anybody and help us with this problem.

 

With regards