This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I am using TMS320F28388D controller, i would like to know the status register values of CPU2 after booting in CPU1 using the register CPU2TOCPU1IPCBOOTSTS
.
From the TRM section 5.7.11.2 CPU2 Booting Status I see the values provided, but when I try to observe the values in CCS in debug mode after booting i see only zeros none have been set. How to know if the register values are set or not.
I have this code 'Device_bootCPU2(BOOTMODE_BOOT_TO_FLASH_SECTOR0);' basically I am expecting to see if the CPU2 has booted correctly or not
thanks,
Nagesh
Hello
Make sure CPU2 is actually running through boot ROM. You won't see this when loading the CPU2 app via CCS.
What you want to do it:
Best regards
Chris