Part Number: TMS320F280045
Tool/software: Code Composer Studio
Hi,
We have problems running the code from flash.
We are programing a f280049C processor with the same code, we check in CCS debugger if the code is in flash. The functions are in flash section (0x8000 – 0x9FFF). Then we programmed the f280045 unit, the issue is the code is not running from flash when the unit is in stand-alone mode.
Code Composer Studio 10.0.0.00010
C2800 Compiler Tools 20.2.1 com.ti.cgt.c2000.19.win32.feature.group Texas Instruments