Part Number: TMS320C28346
Hi expert,
My customer use C28346 with external NORFLASH S29AL016(using XINTF).
however, they meet a problem, that when erasing the flash, the SCI interrupt can not be responese.
they did not disable the interrupt. and since the erasing flash need too much time, they want to use SCI interrupt to check the status.
I confirmed with customer they did not use XINTF interrupt. they put it in the thread.
and the SCI interrupt is enabled as shown in the register.
could you kindly point out the method to get the interrupt respones while erasing the flash?
BR
Emma