Part Number: TMS320F280048C
Application loaded on to flash via CCS debug port works fine. I need to dataload the application on to flash via SCI boot on F28004x launchpad board. In the application, RED/GREEN LEDs are made to blink every second.
When I select 'Verify', I see the below messages:
Bit rate /s of transfer was: 6616.629883
Application load successful!
Done waiting for application to download and boot...
SUCCESS of Command
ERROR Status: VERIFY_ERROR
ERROR Address: 0x80000
When I select 'DFU', I see the below messages:
Bit rate /s of transfer was: 7375.351074
Application load successful!
Done waiting for application to download and boot...
SUCCESS of Command
ERROR Status: PROGRAM_ERROR
ERROR Address: 0x7200
I need to understand what could be causing this error.
The application boot file generated using hex utility with options --boot --sci8 --ascii
Let me know if need more information.
Please help. With Regards,
Sandeep