This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: F021_API_F2837xD_FPU32.lib in EABI format

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

Hi sirs,

While I am trying to compile my project using the given flash API, I obtain the following error in case of using EABI

#10373-D library "../flash_api/lib/F021_API_F2837xD_FPU32.lib" contains TI-COFF object files which are incompatible with the ELF output file. Ensure you are using the proper library. QuasarPlatform_cpu_pri C/C++ Problem

There is an alternative library compatible with ELF output files?

Thanks in advance

Bernat Feixas