Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM
I would like to purchase your C2000 F28069 control card with DRV 8305 driver board. Also suggest me a compatible PMSM motor with sinusoidal back EMF waveform to verify FOC algorithm on the hardware. If I can get the control card, driver board and motor (motor and dyno) as a kit, it would be great. I plan to use Matlab for the software development. And would be using Field Oriented Control Algorithm for Position control. The motor should be able to rotate full 360 degrees without any special assistance and also I would like to have a position encoder with the motor.