This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28335: 100 pin connector

Part Number: TMDSCNCD28335
Other Parts Discussed in Thread: TMDSHSECDOCK

Hi,

I am trying to find a replacement 100 pin connector for the TI board I tried searching for the Molex connector (0876301001)  and the TE Connectivity(TMDSCNCD28335)  but both seem to be obsolete without any information about a replacement connector.  Is there any alternate connector that can be used ?

Thanks,

Aditya

  • Hi Aditya,

    Unfortunately, you are correct that these connectors are now obsolete in the industy.

    We're reached out & unfortunately are not aware of any alternate manufacturers.  And if there were any, they would require a high Minimum Order Quantity.

    If this is for F28335 device evaluation or a prototype system, we'd recommend to design the F28335 & its supporting circuitry directly onto your board.  Or manufacture your own controller card with a connector you desire.


    Note that for C2000's newer device family's controlCARD we have switched to a newer & more manufacture-able connector in the HSEC8 format from Samtec.  You can refer to the TMDSHSECDOCK for an example baseboard.  This works with the newer F28379D, F280049C, F28388D, and F280025C controlCARDs.

    Sorry not to provide the good news you were likely hoping for. 


    Thank you,
    Brett