Part Number: DRV8301-HC-C2-KIT
Other Parts Discussed in Thread: TMS320F28035, MOTORWARE
The goal is to implement a BLDC motor with sensorless FOC (speed controlled).
Currently we are using the DRV8301-HC-C2-KIT with the Piccolo TMS320F28035 isolated control card.
As a solution we have considered to install the following controlCARD on the board instead:
www.ti.com/.../TMDSCNCD28069MISO
The idea was that the underlying MotorWare (www.ti.com/.../MOTORWARE
would support the ControlCard incl. InstaSPIN-FOC and the corresponding driver (48V/60-100A suitable) would not need to be changed.
Is there anything to be said against this from a technical point of view? Is this combination possible?
Translated with www.DeepL.com/Translator (free version)