Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi all:
I am now working on commnucating with MRF89XA module through SPI interface with Launchpad board.
However, I meet some problems:
1. The configuration of SPI interface on LaunchPad. I want to make sure the SPI interface is : 1MHz,8-bit, SPI mode 0 .
GPIO_setPadConfig(DEVICE_GPIO_PIN_SPISIMOA,GPIO_PIN_TYPE_PULLUP);
GPIO_setPinConfig(DEVICE_GPIO_CFG_SPISIMOA);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPISIMOA,GPIO_QUAL_ASYNC);
//SCLK----GPIO56
GPIO_setPadConfig(DEVICE_GPIO_PIN_SPICLKA,GPIO_PIN_TYPE_PULLUP);
GPIO_setPinConfig(DEVICE_GPIO_CFG_SPICLKA);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPICLKA,GPIO_QUAL_ASYNC);
//SOMI----GPIO17
GPIO_setPadConfig(DEVICE_GPIO_PIN_SPISOMIA,GPIO_PIN_TYPE_STD);
GPIO_setPinConfig(DEVICE_GPIO_CFG_SPISOMIA);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SPISOMIA,GPIO_QUAL_ASYNC);
//SPI_CS----GPIO39
GPIO_setPinConfig(GPIO_39_GPIO39);
GPIO_setPadConfig(39,GPIO_PIN_TYPE_PULLUP);
GPIO_setDirectionMode(39,GPIO_DIR_MODE_OUT);
void initSPI_A()
{
//
// Must put SPI into reset before configuring it.
//
SPI_disableModule(SPIA_BASE);
//
// SPI configuration. Use a 1MHz SPICLK and 8-bit word size,SPI mode 0
//
SPI_setConfig(SPIA_BASE, DEVICE_LSPCLK_FREQ, SPI_PROT_POL0PHA0,
SPI_MODE_MASTER, 1000000, 8);
//
// Configuration complete. Enable the module.
//
SPI_enableModule(SPIA_BASE);
}
2. The Interrupt mechanism:
I am not sure that the write and read function are correct. In "ReadData" function, thr for loop confused me so much. Why do you add "SPI_writeDataBlockingNonFIFO(SPIA_BASE, 0x0000)" to "Send dummy data to receive the EEPROM data". Is this step necessary?? and what does it for?
My peripheral is a RF module but not an eeprom, I have checked the data sheet of RF module,maybe the step "Send dummy data to receive the EEPROM data" is not necessary?
void readData(uint16_t address, uint16_t * data, uint16_t length)
{
uint16_t i;
CSCON_TXLOW;
//
// Send the MSB of the address of the EEPROM
//
/*
SPI_writeDataBlockingNonFIFO(SPIA_BASE, (address & 0xFF00));
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
*/
//
// Send the LSB of the address of the EEPROM
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, (address<<8) );
//
// Dummy read to clear INT_FLAG.
//
SPI_readDataBlockingNonFIFO(SPIA_BASE);
//
// Read the data from the EEPROM
//
for(i = 0; i < length; i++)
{
//
// Send dummy data to receive the EEPROM data
//
SPI_writeDataBlockingNonFIFO(SPIA_BASE, 0x0000);
data[i] = SPI_readDataBlockingNonFIFO(SPIA_BASE);
}
CSCON_TXHIGH;
}
3. I am always blocking here while Debug:
When I check the datasheet, I find the INT_FLAG should be 1 when transmitting or receiving completely, I think I have successfully send the data but why the "INT_FLAG" not be 1.