Other Parts Discussed in Thread: TMS320F28069, CONTROLSUITE
Hello,
I am using a TMS320F28069 and I have a question about the clock definition of the ADC and the other peripherals.
I am using the example F2806x ADC Start-Of-Conversion (SOC) Example Program
From the code it seams to be using the internal oscillator to run at 80MHz.
And the configuration of the ADC clock, its with the next code, is it correct?
SysCtrlRegs.LOSPCP.all = 0x0002;
SysCtrlRegs.XCLK.bit.XCLKOUTDIV=2;
Will this make the ADC clock run at 40MHz?
Cheers,
Filipe Teixeira