This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC Register Maximum value

Hello,

I am using a 28069 control card and the example F2806x ADC Start-Of-Conversion (SOC) Example Program.

I have also tried the same example on a control stick with the 28069 and got also the following results.

I then connect the two ADC input pins of the example to 3V3, the values in the ADC register value only go up to around 4022, should it no be 4095?

If I put one of the input to 3v3 and another to GND, the adc value is 4042 and 0.

The calibration register is updated with the TI value.

Has anyone have the same situation?

 

Best regards,

Filipe Teixeira