This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28075: can't write HIBBOOTMODE

Part Number: TMS320F28075

I need to set a value in RAM memory after WD reset. Due to all RAM memory is cleared, I am trying to use HIBBOOTMODE register to do so.

When I try to write that register, its value doesn't chage, it keeps being 0xF. What should I do to be able to write it?

Register is not locked: CpuSysRegs.CPUSYSLOCK1.bit.HIBBOOTMODE  = 0;

Regards, 

Paloma