Part Number: F28M35H52C
Tool/software: Code Composer Studio
I have tried to load an executable 1 to one sector of flash and then load another executable 2 to the rest of flash.
This has now caused the sector that executable 1 was to be placed to be locked up.
The error I get when I try and reprogram the chip.
I have looked into the security features and am pretty sure that I had not done anything to trigger those.
I have tried "erasing" the sector with the memory fill but it wouldn't validate the input I gave it
altered the gel file to R/W as that was set only to R despite me not having messed with it before and not having issues
I am unsure what is causing this and am hoping someone else may have come across this Unknown error. any help would be appreciated.