Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi
I am doing a project in which I have to generate a modulated sine wave greater than 30 kHz and at the same time receive a signal of the same frequency order using the F28379D board. I have looked at the examples found in c2000 ware about the ADC, I see that there are several types but I am not sure which would be the best for my case. I would appreciate if someone can advise me on which one is more optimal to use.
THANKS