This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320f2806x XCLKOUT

Hi,

The current datasheet (SPRS698A) shows XCLKOUT Max to be 15MHz for these 80MHz devices.

Will this/(should this) XCLKOUT Max be changed to 20MHz, or is there an I/O buffer limitation limiting to 15MHz?

With an 80MHz SYSCLK & /4 as the maximum divider, this would seem to limit running the device at 60MHz if XCLKOUT is needed.

Thanks,
Ian