This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377D: Copy GPIO signals to another GPIO output pins

Part Number: TMS320F28377D

Tool/software: Code Composer Studio

Hi,

I have two PWM signals, PWM1 and PWM2 which are generated using "/* Model initialize function */". I want to read the states of pins (GPIO0 for PWM1A & GPIO2 for PWM2A) and writing them back out in pins (GPIO4 as PWM3A and GPIO5 as PWM3B) without the need to initialise PWM3. I used different GPIO registers as can be shown in the code below but I am not exactly getting the same signals produced by GPIO0 and GPIO2. There is some delay in signals output from GPIO4 and GPIO5 and sometimes at specific duty cycles when I changed the values of the CAMP registers of PWM1 and PWM2, I don't get any output signals from pins GPIO4 and GPIO5. So please help me out? 

#include "StackedTwoPhase.h"
#include "StackedTwoPhase_private.h"

/* Block signals (default storage) */
B_StackedTwoPhase_T StackedTwoPhase_B;

/* Real-time model */
RT_MODEL_StackedTwoPhase_T StackedTwoPhase_M_;
RT_MODEL_StackedTwoPhase_T *const StackedTwoPhase_M = &StackedTwoPhase_M_;

/* Model step function */
void StackedTwoPhase_step(void)
{
/* local block i/o variables */
real_T rtb_TMPRRD;


/* S-Function (c280xgpio_di): '<Root>/Digital Input' */
{

StackedTwoPhase_B.I1 = GpioDataRegs.GPADAT.bit.GPIO0;

}

/* S-Function (c280xgpio_di): '<Root>/Digital Input1' */
{

StackedTwoPhase_B.I2 = GpioDataRegs.GPADAT.bit.GPIO2;

}

/* MATLAB Function: '<Root>/MATLAB Function1' incorporates:
* Constant: '<Root>/Constant'
*/




/* End of MATLAB Function: '<Root>/MATLAB Function1' */

/* S-Function (c280xgpio_do): '<Root>/Digital Output' */
{

if (StackedTwoPhase_B.I1)

GpioDataRegs.GPASET.bit.GPIO4=1;

else

GpioDataRegs.GPACLEAR.bit.GPIO4=1;

}

/* S-Function (c280xgpio_do): '<Root>/Digital Output1' */
{

if (StackedTwoPhase_B.I2)

GpioDataRegs.GPASET.bit.GPIO5=1;

else

GpioDataRegs.GPACLEAR.bit.GPIO5=1;

}

/* Gain: '<Root>/TMPRRD' incorporates:
* Constant: '<Root>/Constant'
*/
rtb_TMPRRD = StackedTwoPhase_P.TMPRRD_Gain * StackedTwoPhase_P.Constant_Value;

/* S-Function (c2802xpwm): '<Root>/ePWM1' */

/*-- Update CMPA value for ePWM1 --*/
{
EPwm1Regs.CMPA.bit.CMPA = (uint16_T)(rtb_TMPRRD);
}

/* S-Function (c2802xpwm): '<Root>/ePWM2' incorporates:
* Constant: '<Root>/Phase_2'
*/
EPwm2Regs.TBPHS.bit.TBPHS = 499;

/*-- Update CMPA value for ePWM2 --*/
{
EPwm2Regs.CMPA.bit.CMPA = (uint16_T)(rtb_TMPRRD);
}
}

/* Model initialize function */
void StackedTwoPhase_initialize(void)
{
/* Registration code */




/* Start for S-Function (c280xgpio_do): '<Root>/Digital Output' */
EALLOW;
GpioCtrlRegs.GPADIR.bit.GPIO4 = 1;

EDIS;

/* Start for S-Function (c280xgpio_do): '<Root>/Digital Output1' */
EALLOW;
GpioCtrlRegs.GPADIR.bit.GPIO5 = 1;

EDIS;
/* Start for S-Function (c2802xpwm): '<Root>/ePWM1' */
EALLOW;
CpuSysRegs.PCLKCR2.bit.EPWM1 = 1;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;

/*** Initialize ePWM1 modules ***/
{
/* // Time Base Control Register
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // Counter Mode
EPwm1Regs.TBCTL.bit.SYNCOSEL = 1; // Sync Output Select
EPwm1Regs.TBCTL.bit.PRDLD = 0; // Shadow select
EPwm1Regs.TBCTL.bit.PHSEN = 0; // Phase Load Enable
EPwm1Regs.TBCTL.bit.PHSDIR = 0; // Phase Direction Bit
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // High Speed TBCLK Pre-scaler
EPwm1Regs.TBCTL.bit.CLKDIV = 0; // Time Base Clock Pre-scaler
EPwm1Regs.TBCTL.bit.SWFSYNC = 0; // Software Force Sync Pulse
*/
EPwm1Regs.TBCTL.all = (EPwm1Regs.TBCTL.all & ~0x3FFF) | 0x10;

/*-- Setup Time-Base (TB) Submodule --*/
EPwm1Regs.TBPRD = 999; // Time Base Period Register

/* // Time-Base Phase Register
EPwm1Regs.TBPHS.bit.TBPHS = 0; // Phase offset register
*/
EPwm1Regs.TBPHS.all = (EPwm1Regs.TBPHS.all & ~0xFFFF0000) | 0x0;

// Time Base Counter Register
EPwm1Regs.TBCTR = 0x0000; /* Clear counter*/

/*-- Setup Counter_Compare (CC) Submodule --*/
/* // Counter Compare Control Register
EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // Compare A Register Block Operating Mode
EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0; // Compare B Register Block Operating Mode
EPwm1Regs.CMPCTL.bit.LOADAMODE = 0; // Active Compare A Load
EPwm1Regs.CMPCTL.bit.LOADBMODE = 0; // Active Compare B Load
*/
EPwm1Regs.CMPCTL.all = (EPwm1Regs.CMPCTL.all & ~0x5F) | 0x0;

/* EPwm1Regs.CMPCTL2.bit.SHDWCMODE = 0; // Compare C Register Block Operating Mode

EPwm1Regs.CMPCTL2.bit.SHDWDMODE = 0; // Compare D Register Block Operating Mode
*/
EPwm1Regs.CMPCTL2.all = (EPwm1Regs.CMPCTL2.all & ~0x50) | 0x0;
EPwm1Regs.CMPA.bit.CMPA = 0; // Counter Compare A Register
EPwm1Regs.CMPB.bit.CMPB = 0; // Counter Compare B Register
EPwm1Regs.CMPC = 0; // Counter Compare C Register
EPwm1Regs.CMPD = 0; // Counter Compare D Register

/*-- Setup Action-Qualifier (AQ) Submodule --*/
EPwm1Regs.AQCTLA.all = 33; // Action Qualifier Control Register For Output A
EPwm1Regs.AQCTLB.all = 33; // Action Qualifier Control Register For Output B

/* // Action Qualifier Software Force Register
EPwm1Regs.AQSFRC.bit.RLDCSF = 0; // Reload from Shadow Options
*/
EPwm1Regs.AQSFRC.all = (EPwm1Regs.AQSFRC.all & ~0xC0) | 0x0;

/* // Action Qualifier Continuous S/W Force Register
EPwm1Regs.AQCSFRC.bit.CSFA = 0; // Continuous Software Force on output A
EPwm1Regs.AQCSFRC.bit.CSFB = 0; // Continuous Software Force on output B
*/
EPwm1Regs.AQCSFRC.all = (EPwm1Regs.AQCSFRC.all & ~0xF) | 0x0;

/*-- Setup Dead-Band Generator (DB) Submodule --*/
/* // Dead-Band Generator Control Register
EPwm1Regs.DBCTL.bit.OUT_MODE = 3; // Dead Band Output Mode Control
EPwm1Regs.DBCTL.bit.IN_MODE = 0; // Dead Band Input Select Mode Control
EPwm1Regs.DBCTL.bit.POLSEL = 2; // Polarity Select Control
EPwm1Regs.DBCTL.bit.HALFCYCLE = 0; // Half Cycle Clocking Enable
*/
EPwm1Regs.DBCTL.all = (EPwm1Regs.DBCTL.all & ~0x803F) | 0xB;
EPwm1Regs.DBRED.bit.DBRED = 20; // Dead-Band Generator Rising Edge Delay Count Register
EPwm1Regs.DBFED.bit.DBFED = 20; // Dead-Band Generator Falling Edge Delay Count Register

/*-- Setup Event-Trigger (ET) Submodule --*/
/* // Event Trigger Selection and Pre-Scale Register
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Start of Conversion A Enable
EPwm1Regs.ETSEL.bit.SOCASELCMP = 0;
EPwm1Regs.ETSEL.bit.SOCASEL = 4 ; // Start of Conversion A Select
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // EPWM1SOCA Period Select

EPwm1Regs.ETSEL.bit.SOCBEN = 0; // Start of Conversion B Enable

EPwm1Regs.ETSEL.bit.SOCBSELCMP = 0;
EPwm1Regs.ETSEL.bit.SOCBSEL = 1; // Start of Conversion A Select
EPwm1Regs.ETPS.bit.SOCBPRD = 1; // EPWM1SOCB Period Select
EPwm1Regs.ETSEL.bit.INTEN = 0; // EPWM1INTn Enable
EPwm1Regs.ETSEL.bit.INTSELCMP = 0;
EPwm1Regs.ETSEL.bit.INTSEL = 4; // Start of Conversion A Select

EPwm1Regs.ETPS.bit.INTPRD = 1; // EPWM1INTn Period Select
*/
EPwm1Regs.ETSEL.all = (EPwm1Regs.ETSEL.all & ~0xFF7F) | 0x1C04;
EPwm1Regs.ETPS.all = (EPwm1Regs.ETPS.all & ~0x3303) | 0x1101;

/*-- Setup PWM-Chopper (PC) Submodule --*/
/* // PWM Chopper Control Register
EPwm1Regs.PCCTL.bit.CHPEN = 0; // PWM chopping enable
EPwm1Regs.PCCTL.bit.CHPFREQ = 0; // Chopping clock frequency
EPwm1Regs.PCCTL.bit.OSHTWTH = 0; // One-shot pulse width
EPwm1Regs.PCCTL.bit.CHPDUTY = 0; // Chopping clock Duty cycle
*/
EPwm1Regs.PCCTL.all = (EPwm1Regs.PCCTL.all & ~0x7FF) | 0x0;

/*-- Set up Trip-Zone (TZ) Submodule --*/
EALLOW;
EPwm1Regs.TZSEL.all = 0; // Trip Zone Select Register

/* // Trip Zone Control Register
EPwm1Regs.TZCTL.bit.TZA = 3; // TZ1 to TZ6 Trip Action On EPWM1A
EPwm1Regs.TZCTL.bit.TZB = 3; // TZ1 to TZ6 Trip Action On EPWM1B
EPwm1Regs.TZCTL.bit.DCAEVT1 = 3; // EPWM1A action on DCAEVT1
EPwm1Regs.TZCTL.bit.DCAEVT2 = 3; // EPWM1A action on DCAEVT2
EPwm1Regs.TZCTL.bit.DCBEVT1 = 3; // EPWM1B action on DCBEVT1
EPwm1Regs.TZCTL.bit.DCBEVT2 = 3; // EPWM1B action on DCBEVT2
*/
EPwm1Regs.TZCTL.all = (EPwm1Regs.TZCTL.all & ~0xFFF) | 0xFFF;

/* // Trip Zone Enable Interrupt Register
EPwm1Regs.TZEINT.bit.OST = 0; // Trip Zones One Shot Int Enable
EPwm1Regs.TZEINT.bit.CBC = 0; // Trip Zones Cycle By Cycle Int Enable
EPwm1Regs.TZEINT.bit.DCAEVT1 = 0; // Digital Compare A Event 1 Int Enable
EPwm1Regs.TZEINT.bit.DCAEVT2 = 0; // Digital Compare A Event 2 Int Enable
EPwm1Regs.TZEINT.bit.DCBEVT1 = 0; // Digital Compare B Event 1 Int Enable
EPwm1Regs.TZEINT.bit.DCBEVT2 = 0; // Digital Compare B Event 2 Int Enable
*/
EPwm1Regs.TZEINT.all = (EPwm1Regs.TZEINT.all & ~0x7E) | 0x0;

/* // Digital Compare A Control Register
EPwm1Regs.DCACTL.bit.EVT1SYNCE = 0; // DCAEVT1 SYNC Enable
EPwm1Regs.DCACTL.bit.EVT1SOCE = 1; // DCAEVT1 SOC Enable
EPwm1Regs.DCACTL.bit.EVT1FRCSYNCSEL = 0; // DCAEVT1 Force Sync Signal
EPwm1Regs.DCACTL.bit.EVT1SRCSEL = 0; // DCAEVT1 Source Signal
EPwm1Regs.DCACTL.bit.EVT2FRCSYNCSEL = 0; // DCAEVT2 Force Sync Signal
EPwm1Regs.DCACTL.bit.EVT2SRCSEL = 0; // DCAEVT2 Source Signal
*/
EPwm1Regs.DCACTL.all = (EPwm1Regs.DCACTL.all & ~0x30F) | 0x4;

/* // Digital Compare B Control Register
EPwm1Regs.DCBCTL.bit.EVT1SYNCE = 0; // DCBEVT1 SYNC Enable
EPwm1Regs.DCBCTL.bit.EVT1SOCE = 0; // DCBEVT1 SOC Enable
EPwm1Regs.DCBCTL.bit.EVT1FRCSYNCSEL = 0; // DCBEVT1 Force Sync Signal
EPwm1Regs.DCBCTL.bit.EVT1SRCSEL = 0; // DCBEVT1 Source Signal
EPwm1Regs.DCBCTL.bit.EVT2FRCSYNCSEL = 0; // DCBEVT2 Force Sync Signal
EPwm1Regs.DCBCTL.bit.EVT2SRCSEL = 0; // DCBEVT2 Source Signal
*/
EPwm1Regs.DCBCTL.all = (EPwm1Regs.DCBCTL.all & ~0x30F) | 0x0;

/* // Digital Compare Trip Select Register
EPwm1Regs.DCTRIPSEL.bit.DCAHCOMPSEL = 0; // Digital Compare A High COMP Input Select

EPwm1Regs.DCTRIPSEL.bit.DCALCOMPSEL = 1; // Digital Compare A Low COMP Input Select
EPwm1Regs.DCTRIPSEL.bit.DCBHCOMPSEL = 0; // Digital Compare B High COMP Input Select
EPwm1Regs.DCTRIPSEL.bit.DCBLCOMPSEL = 1; // Digital Compare B Low COMP Input Select





*/
EPwm1Regs.DCTRIPSEL.all = (EPwm1Regs.DCTRIPSEL.all & ~ 0xFFFF) | 0x1010;

/* // Trip Zone Digital Comparator Select Register
EPwm1Regs.TZDCSEL.bit.DCAEVT1 = 0; // Digital Compare Output A Event 1
EPwm1Regs.TZDCSEL.bit.DCAEVT2 = 0; // Digital Compare Output A Event 2
EPwm1Regs.TZDCSEL.bit.DCBEVT1 = 0; // Digital Compare Output B Event 1
EPwm1Regs.TZDCSEL.bit.DCBEVT2 = 0; // Digital Compare Output B Event 2
*/
EPwm1Regs.TZDCSEL.all = (EPwm1Regs.TZDCSEL.all & ~0xFFF) | 0x0;

/* // Digital Compare Filter Control Register
EPwm1Regs.DCFCTL.bit.BLANKE = 0; // Blanking Enable/Disable
EPwm1Regs.DCFCTL.bit.PULSESEL = 1; // Pulse Select for Blanking & Capture Alignment
EPwm1Regs.DCFCTL.bit.BLANKINV = 0; // Blanking Window Inversion
EPwm1Regs.DCFCTL.bit.SRCSEL = 0; // Filter Block Signal Source Select
*/
EPwm1Regs.DCFCTL.all = (EPwm1Regs.DCFCTL.all & ~0x3F) | 0x10;
EPwm1Regs.DCFOFFSET = 0; // Digital Compare Filter Offset Register
EPwm1Regs.DCFWINDOW = 0; // Digital Compare Filter Window Register

/* // Digital Compare Capture Control Register
EPwm1Regs.DCCAPCTL.bit.CAPE = 0; // Counter Capture Enable
*/
EPwm1Regs.DCCAPCTL.all = (EPwm1Regs.DCCAPCTL.all & ~0x1) | 0x0;

/* // HRPWM Configuration Register
EPwm1Regs.HRCNFG.bit.SWAPAB = 0; // Swap EPWMA and EPWMB Outputs Bit
EPwm1Regs.HRCNFG.bit.SELOUTB = 0; // EPWMB Output Selection Bit
*/
EPwm1Regs.HRCNFG.all = (EPwm1Regs.HRCNFG.all & ~0xA0) | 0x0;

/* Update the Link Registers with the link value for all the Compare values and TBPRD */
/* No error is thrown if the ePWM register exists in the model or not */
EPwm1Regs.EPWMXLINK.bit.TBPRDLINK = 0;
EPwm1Regs.EPWMXLINK.bit.CMPALINK = 0;
EPwm1Regs.EPWMXLINK.bit.CMPBLINK = 0;
EPwm1Regs.EPWMXLINK.bit.CMPCLINK = 0;
EPwm1Regs.EPWMXLINK.bit.CMPDLINK = 0;
EDIS;
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
}

/* Start for S-Function (c2802xpwm): '<Root>/ePWM2' incorporates:
* Constant: '<Root>/Phase_2'
*/
EALLOW;
CpuSysRegs.PCLKCR2.bit.EPWM2 = 1;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;

/*** Initialize ePWM2 modules ***/
{
/* // Time Base Control Register
EPwm2Regs.TBCTL.bit.CTRMODE = 0; // Counter Mode
EPwm2Regs.TBCTL.bit.SYNCOSEL = 0; // Sync Output Select
EPwm2Regs.TBCTL.bit.PRDLD = 0; // Shadow select
EPwm2Regs.TBCTL.bit.PHSEN = 1; // Phase Load Enable
EPwm2Regs.TBCTL.bit.PHSDIR = 0; // Phase Direction Bit
EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; // High Speed TBCLK Pre-scaler
EPwm2Regs.TBCTL.bit.CLKDIV = 0; // Time Base Clock Pre-scaler
EPwm2Regs.TBCTL.bit.SWFSYNC = 0; // Software Force Sync Pulse
*/
EPwm2Regs.TBCTL.all = (EPwm2Regs.TBCTL.all & ~0x3FFF) | 0x4;

/*-- Setup Time-Base (TB) Submodule --*/
EPwm2Regs.TBPRD = 999; // Time Base Period Register

/* // Time-Base Phase Register
EPwm2Regs.TBPHS.bit.TBPHS = 0; // Phase offset register
*/
EPwm2Regs.TBPHS.all = (EPwm2Regs.TBPHS.all & ~0xFFFF0000) | 0x0;

// Time Base Counter Register
EPwm2Regs.TBCTR = 0x0000; /* Clear counter*/

/*-- Setup Counter_Compare (CC) Submodule --*/
/* // Counter Compare Control Register
EPwm2Regs.CMPCTL.bit.SHDWAMODE = 0; // Compare A Register Block Operating Mode
EPwm2Regs.CMPCTL.bit.SHDWBMODE = 0; // Compare B Register Block Operating Mode
EPwm2Regs.CMPCTL.bit.LOADAMODE = 0; // Active Compare A Load
EPwm2Regs.CMPCTL.bit.LOADBMODE = 0; // Active Compare B Load
*/
EPwm2Regs.CMPCTL.all = (EPwm2Regs.CMPCTL.all & ~0x5F) | 0x0;

/* EPwm2Regs.CMPCTL2.bit.SHDWCMODE = 0; // Compare C Register Block Operating Mode

EPwm2Regs.CMPCTL2.bit.SHDWDMODE = 0; // Compare D Register Block Operating Mode
*/
EPwm2Regs.CMPCTL2.all = (EPwm2Regs.CMPCTL2.all & ~0x50) | 0x0;
EPwm2Regs.CMPA.bit.CMPA = 0; // Counter Compare A Register
EPwm2Regs.CMPB.bit.CMPB = 0; // Counter Compare B Register
EPwm2Regs.CMPC = 0; // Counter Compare C Register
EPwm2Regs.CMPD = 0; // Counter Compare D Register

/*-- Setup Action-Qualifier (AQ) Submodule --*/
EPwm2Regs.AQCTLA.all = 97; // Action Qualifier Control Register For Output A
EPwm2Regs.AQCTLB.all = 33; // Action Qualifier Control Register For Output B

/* // Action Qualifier Software Force Register
EPwm2Regs.AQSFRC.bit.RLDCSF = 0; // Reload from Shadow Options
*/
EPwm2Regs.AQSFRC.all = (EPwm2Regs.AQSFRC.all & ~0xC0) | 0x0;

/* // Action Qualifier Continuous S/W Force Register
EPwm2Regs.AQCSFRC.bit.CSFA = 0; // Continuous Software Force on output A
EPwm2Regs.AQCSFRC.bit.CSFB = 0; // Continuous Software Force on output B
*/
EPwm2Regs.AQCSFRC.all = (EPwm2Regs.AQCSFRC.all & ~0xF) | 0x0;

/*-- Setup Dead-Band Generator (DB) Submodule --*/
/* // Dead-Band Generator Control Register
EPwm2Regs.DBCTL.bit.OUT_MODE = 3; // Dead Band Output Mode Control
EPwm2Regs.DBCTL.bit.IN_MODE = 0; // Dead Band Input Select Mode Control
EPwm2Regs.DBCTL.bit.POLSEL = 2; // Polarity Select Control
EPwm2Regs.DBCTL.bit.HALFCYCLE = 0; // Half Cycle Clocking Enable
*/
EPwm2Regs.DBCTL.all = (EPwm2Regs.DBCTL.all & ~0x803F) | 0xB;
EPwm2Regs.DBRED.bit.DBRED = 20; // Dead-Band Generator Rising Edge Delay Count Register
EPwm2Regs.DBFED.bit.DBFED = 20; // Dead-Band Generator Falling Edge Delay Count Register

/*-- Setup Event-Trigger (ET) Submodule --*/
/* // Event Trigger Selection and Pre-Scale Register
EPwm2Regs.ETSEL.bit.SOCAEN = 1; // Start of Conversion A Enable
EPwm2Regs.ETSEL.bit.SOCASELCMP = 0;
EPwm2Regs.ETSEL.bit.SOCASEL = 4 ; // Start of Conversion A Select
EPwm2Regs.ETPS.bit.SOCAPRD = 1; // EPWM2SOCA Period Select

EPwm2Regs.ETSEL.bit.SOCBEN = 0; // Start of Conversion B Enable

EPwm2Regs.ETSEL.bit.SOCBSELCMP = 0;
EPwm2Regs.ETSEL.bit.SOCBSEL = 1; // Start of Conversion A Select
EPwm2Regs.ETPS.bit.SOCBPRD = 1; // EPWM2SOCB Period Select
EPwm2Regs.ETSEL.bit.INTEN = 0; // EPWM2INTn Enable
EPwm2Regs.ETSEL.bit.INTSELCMP = 0;
EPwm2Regs.ETSEL.bit.INTSEL = 4; // Start of Conversion A Select

EPwm2Regs.ETPS.bit.INTPRD = 1; // EPWM2INTn Period Select
*/
EPwm2Regs.ETSEL.all = (EPwm2Regs.ETSEL.all & ~0xFF7F) | 0x1C04;
EPwm2Regs.ETPS.all = (EPwm2Regs.ETPS.all & ~0x3303) | 0x1101;

/*-- Setup PWM-Chopper (PC) Submodule --*/
/* // PWM Chopper Control Register
EPwm2Regs.PCCTL.bit.CHPEN = 0; // PWM chopping enable
EPwm2Regs.PCCTL.bit.CHPFREQ = 0; // Chopping clock frequency
EPwm2Regs.PCCTL.bit.OSHTWTH = 0; // One-shot pulse width
EPwm2Regs.PCCTL.bit.CHPDUTY = 0; // Chopping clock Duty cycle
*/
EPwm2Regs.PCCTL.all = (EPwm2Regs.PCCTL.all & ~0x7FF) | 0x0;

/*-- Set up Trip-Zone (TZ) Submodule --*/
EALLOW;
EPwm2Regs.TZSEL.all = 0; // Trip Zone Select Register

/* // Trip Zone Control Register
EPwm2Regs.TZCTL.bit.TZA = 3; // TZ1 to TZ6 Trip Action On EPWM2A
EPwm2Regs.TZCTL.bit.TZB = 3; // TZ1 to TZ6 Trip Action On EPWM2B
EPwm2Regs.TZCTL.bit.DCAEVT1 = 3; // EPWM2A action on DCAEVT1
EPwm2Regs.TZCTL.bit.DCAEVT2 = 3; // EPWM2A action on DCAEVT2
EPwm2Regs.TZCTL.bit.DCBEVT1 = 3; // EPWM2B action on DCBEVT1
EPwm2Regs.TZCTL.bit.DCBEVT2 = 3; // EPWM2B action on DCBEVT2
*/
EPwm2Regs.TZCTL.all = (EPwm2Regs.TZCTL.all & ~0xFFF) | 0xFFF;

/* // Trip Zone Enable Interrupt Register
EPwm2Regs.TZEINT.bit.OST = 0; // Trip Zones One Shot Int Enable
EPwm2Regs.TZEINT.bit.CBC = 0; // Trip Zones Cycle By Cycle Int Enable
EPwm2Regs.TZEINT.bit.DCAEVT1 = 0; // Digital Compare A Event 1 Int Enable
EPwm2Regs.TZEINT.bit.DCAEVT2 = 0; // Digital Compare A Event 2 Int Enable
EPwm2Regs.TZEINT.bit.DCBEVT1 = 0; // Digital Compare B Event 1 Int Enable
EPwm2Regs.TZEINT.bit.DCBEVT2 = 0; // Digital Compare B Event 2 Int Enable
*/
EPwm2Regs.TZEINT.all = (EPwm2Regs.TZEINT.all & ~0x7E) | 0x0;

/* // Digital Compare A Control Register
EPwm2Regs.DCACTL.bit.EVT1SYNCE = 0; // DCAEVT1 SYNC Enable
EPwm2Regs.DCACTL.bit.EVT1SOCE = 1; // DCAEVT1 SOC Enable
EPwm2Regs.DCACTL.bit.EVT1FRCSYNCSEL = 0; // DCAEVT1 Force Sync Signal
EPwm2Regs.DCACTL.bit.EVT1SRCSEL = 0; // DCAEVT1 Source Signal
EPwm2Regs.DCACTL.bit.EVT2FRCSYNCSEL = 0; // DCAEVT2 Force Sync Signal
EPwm2Regs.DCACTL.bit.EVT2SRCSEL = 0; // DCAEVT2 Source Signal
*/
EPwm2Regs.DCACTL.all = (EPwm2Regs.DCACTL.all & ~0x30F) | 0x4;

/* // Digital Compare B Control Register
EPwm2Regs.DCBCTL.bit.EVT1SYNCE = 0; // DCBEVT1 SYNC Enable
EPwm2Regs.DCBCTL.bit.EVT1SOCE = 0; // DCBEVT1 SOC Enable
EPwm2Regs.DCBCTL.bit.EVT1FRCSYNCSEL = 0; // DCBEVT1 Force Sync Signal
EPwm2Regs.DCBCTL.bit.EVT1SRCSEL = 0; // DCBEVT1 Source Signal
EPwm2Regs.DCBCTL.bit.EVT2FRCSYNCSEL = 0; // DCBEVT2 Force Sync Signal
EPwm2Regs.DCBCTL.bit.EVT2SRCSEL = 0; // DCBEVT2 Source Signal
*/
EPwm2Regs.DCBCTL.all = (EPwm2Regs.DCBCTL.all & ~0x30F) | 0x0;

/* // Digital Compare Trip Select Register
EPwm2Regs.DCTRIPSEL.bit.DCAHCOMPSEL = 0; // Digital Compare A High COMP Input Select

EPwm2Regs.DCTRIPSEL.bit.DCALCOMPSEL = 1; // Digital Compare A Low COMP Input Select
EPwm2Regs.DCTRIPSEL.bit.DCBHCOMPSEL = 0; // Digital Compare B High COMP Input Select
EPwm2Regs.DCTRIPSEL.bit.DCBLCOMPSEL = 1; // Digital Compare B Low COMP Input Select





*/
EPwm2Regs.DCTRIPSEL.all = (EPwm2Regs.DCTRIPSEL.all & ~ 0xFFFF) | 0x1010;

/* // Trip Zone Digital Comparator Select Register
EPwm2Regs.TZDCSEL.bit.DCAEVT1 = 0; // Digital Compare Output A Event 1
EPwm2Regs.TZDCSEL.bit.DCAEVT2 = 0; // Digital Compare Output A Event 2
EPwm2Regs.TZDCSEL.bit.DCBEVT1 = 0; // Digital Compare Output B Event 1
EPwm2Regs.TZDCSEL.bit.DCBEVT2 = 0; // Digital Compare Output B Event 2
*/
EPwm2Regs.TZDCSEL.all = (EPwm2Regs.TZDCSEL.all & ~0xFFF) | 0x0;

/* // Digital Compare Filter Control Register
EPwm2Regs.DCFCTL.bit.BLANKE = 0; // Blanking Enable/Disable
EPwm2Regs.DCFCTL.bit.PULSESEL = 1; // Pulse Select for Blanking & Capture Alignment
EPwm2Regs.DCFCTL.bit.BLANKINV = 0; // Blanking Window Inversion
EPwm2Regs.DCFCTL.bit.SRCSEL = 0; // Filter Block Signal Source Select
*/
EPwm2Regs.DCFCTL.all = (EPwm2Regs.DCFCTL.all & ~0x3F) | 0x10;
EPwm2Regs.DCFOFFSET = 0; // Digital Compare Filter Offset Register
EPwm2Regs.DCFWINDOW = 0; // Digital Compare Filter Window Register

/* // Digital Compare Capture Control Register
EPwm2Regs.DCCAPCTL.bit.CAPE = 0; // Counter Capture Enable
*/
EPwm2Regs.DCCAPCTL.all = (EPwm2Regs.DCCAPCTL.all & ~0x1) | 0x0;

/* // HRPWM Configuration Register
EPwm2Regs.HRCNFG.bit.SWAPAB = 0; // Swap EPWMA and EPWMB Outputs Bit
EPwm2Regs.HRCNFG.bit.SELOUTB = 0; // EPWMB Output Selection Bit
*/
EPwm2Regs.HRCNFG.all = (EPwm2Regs.HRCNFG.all & ~0xA0) | 0x0;

/* Update the Link Registers with the link value for all the Compare values and TBPRD */
/* No error is thrown if the ePWM register exists in the model or not */
EPwm2Regs.EPWMXLINK.bit.TBPRDLINK = 1;
EPwm2Regs.EPWMXLINK.bit.CMPALINK = 1;
EPwm2Regs.EPWMXLINK.bit.CMPBLINK = 1;
EPwm2Regs.EPWMXLINK.bit.CMPCLINK = 1;
EPwm2Regs.EPWMXLINK.bit.CMPDLINK = 1;
EDIS;
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
}
}

/* Model terminate function */
void StackedTwoPhase_terminate(void)
{
/* (no terminate code required) */
}

/*
* File trailer for generated code.
*
* [EOF]
*/

  • Mohammed,

    I'm a bit confused how are you copying the signal? by reading GPIO state and writing it back out?

    Nima

  • Hi Nima,

    Thanks for your reply.

    Yes, I mean reading the states of pins GPIO0 and GPIO2 and writing them back out in pins GPIO4 and GPIO5 with no delay. When I change the CMPA values to change the duty cycle from 0.1 to 0.9 for ePWM1 and ePWM2, for some values I don’t see any signals in pins GPIO04 and GPIO05 and with other values, I get different signals than the required signals of pins GPIO0 and GPIO2. Btw, there is a phase shift between signals ePWM1 and ePWM2. Please see the new uploaded picture.

    I am also using the embedded support package in MATLAB to generate the code.

    regards,

    Mohammed

  • Mohammed, 

    What you are doing WILL ALWAYS have a delay. For the signal to go through the GPIO input circuit, then be read through sw, then write back out through SW, then go through GPIO output circuit, you will always have this delay.

    Nima

  • Nima,

    I appreciate your time and response. I understand!

    To be honest my main aim is to actually combine and compare two PWM signals e.g. PWM1A and PWM2A to get third PWM signals which are PWM3A & and PWM3B.

    In other words, I want to compare the two signals using Gate Logics. For example:

    (PWM1A XOR PWM2A = PWM3A), and (PWM1A  NXOR PWM2A = ePWM3B).

    Hence, I thought of using the GPIO pins as input and output signals. So can you please advise me of a more efficient way?

    Regards,

    Mohammed

  • Mohammed Alharbi said:

    To be honest my main aim is to actually combine and compare two PWM signals e.g. PWM1A and PWM2A to get third PWM signals which are PWM3A & and PWM3B.

    In other words, I want to compare the two signals using Gate Logics. For example:

    (PWM1A XOR PWM2A = PWM3A), and (PWM1A  NXOR PWM2A = ePWM3B).

    PERFECT, now that I know what you are trying to do I can guide you much better.

    YOU MUST USE THE CLB, the CLB is perfect for this.

    You have access to EPWM1,2,3 through the CLB, you can use the EPWM1A and EPWM2A as inputs to a CLB TILE (Use CLB3), then implement your logic inside  a LUT of the CLB module, then output your signal onto EPWM3A through the CLB OUTPUT INTERSECT (override).

    It will have no delay. Build in hardware support.

    Nima

  • There are mountain of CLB documentations (user guide, application reports, etc) + video tutorials on training.ti.com + over 20 examples (driverlib based).

    Nima

  • Thanks Nima for your help. I will try to look at how to do them using the proposed method.

    Regards,

    Mohammed

  • You are welcome Mohammed.