Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28379D
Tool/software: Code Composer Studio
Dear TI experts,
We developed a project on the launchpad and would like to run it on the control card. I am loading the same code that works well on the TMS320F28379D launchpad to the control card. It stuck at the ILLEGAL_ISR() when I run the program. I am wondering if the control card shares the exact same configurations (includes, linkers, memory map, and etc.) as the launchpad? If there are differences between the control card and the launchpad, is there any document I can refer to?
Thank you!