This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: HLC PUSH Behavior

Part Number: TMS320F28379D

Greetings,

I am using the HLC to push data which is retrieved at a later time. In reading the TRM, I find that I am confused about some things.

  1. Section 26.4.6.4 Operation of the PUSH and PULL Instructions: The first paragraph says that the PUSH buffer is mapped at address offset 0x200. From what is this offset applied?
  2. Section 26.6.3.8 CLB_BUF_PTR: The information on the PUSH field indicates that it is the number of values which have been pulled from the buffer by the HLC. Is this correct, or is it the number which have been pushed by the HLC? My observations say it’s the latter. Same question for the PULL field.
  3. Typo in paragraph 3 of 26.4.6.4. “the CPU can at any time” s.b. “the CPU at any time”.

Thank you,

Ed