Part Number: TMS320F28335
Hello,
customer is programming the F28335 in production over the bootloader and the flash API v2.10 which is loaded into the RAM and then flashing the firmware. After code verification 1% of the device returns „STATUS_FAIL_VERIFY“. Further failure messages are: FirstFailAddr, ExpectedData und ActualData. Nevertheless it seems that the programming was ok and the device is running well. But customer still worries about the message and change the F28335 with a new one because he fears failures in the field later. What could be the reason for this verified failed messages?
Regards, Holger