Part Number: TMS320F280049C
Both instaspin-FOC and instaspin-Motion use Fast software encoder. i have several questions about Fast as follow:
1. in the control diagram, Fast need the motor phase voltage samples(va,vb,vb), but in most cases, inverters often drive motor directly, so the phase voltage waveform is something like PWM not a 'sine' wave, does Fast really need the PWM waveform or just use the generated AC waveform from algorithm to calculate rotor angle
2. what is the limitation of frequency for 'Fast', can it work in a high frequency, as 1kHz?
3. in the user guide, it is said that injection technology has been used in algorithm, can this program run in the ram, is there a lib in the motor control SDK