Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
Hi Guys. I've made my own breakout board for my F28335 176PIN. My F28335 won't go out of LIMP Mode. I've checked the power rails 3.3V for I/O and 2.1V for CPU.
I have a 20Mhz crystal connected to pins 104 X1 and 102 X2 the other side connected to 15pf ceramic capacitors to GND.
CCS9 downloads my Assembler code to RAM fine with no errors. I have connected a LCD to PORTB so I can read values of the internal F28335 registers. LCD is working fine as well.
I then realised that the F28335 is running very slowly. I read the PLLSTS register in Assembler ( I'm an Assembler guy ) and it tells me LIMP mode is on. I read the XCLKOUT pin 138 with my scope and it says 1.00Mhz speed.
I would have though connecting the 20Mhz crystal would make it run at 20Mhz / 4 = 5Mhz but no, it's only running at 1Mhz.
Can someone please let me know what I missed in setting up the F28335 properly.
Thanks guys, hope to hear from you soon.
Peter