This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

re: inverter using f2808 and dmc 550

Hello everyone,

I bought an ezdsp f2808 kit and dmc 550 to make an inverter. I was encouraged to buy these parts to follow a document from TI groups. They have this document " Digital implementation of a DC-AC single phase power supply".  There are some revisions on the components and assumed that they are already fix before delivery. So I followed this document, as well as the demonstration figure to run these kits.

But until now I can't successfully run the machine. I'm just downloading exactly the sample project that was from the system document but it has still errors while running. There is no exact procedure on the hardware connection if what is the first part to be connected to the kit, the +5V source or the dc power supply?

Could anyone who had tried running this sample project and done it succesfully, could you please help me where did I go wrong? I don't know where to troubleshoot this kit.

thanks,

jo