Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Good Day
I'm trying to get a project running on my computer, but I can't fix these 5 warnings.
As mentioned here, I made sure that "F2837xD_Headers_nonBIOS_cpu1.cmd" is included in the linker configurations as well as "2837xD_RAM_lnk_cpu1.cmd".
How can I fix these warnings, which other files have to be included as well? I am running CCS 10.1.1.00004 with C2000Ware 3.3.0 and the compiler version V20.2.1.LTS.
Description Resource Path Location Type #10247-D creating output section "AdcaResultFile" without a SECTIONS specification #10247-D creating output section "AdcbResultFile" without a SECTIONS specification #10247-D creating output section "AdccResultFile" without a SECTIONS specification #10247-D creating output section "AdcdResultFile" without a SECTIONS specification #10247-D creating output section "Cla1SoftIntRegsFile" without a SECTIONS specification