Part Number: MOTORWARE
Tool/software: Code Composer Studio
I run lab5a program on my fitness bike project using F28069M controlCARD .The generated power is consumed on cement resistance.
The SPMSM motor's parameters have been identified and record parameters in user.h.
If set gMotorVars.IqRef_A positive ,for example _IQ(0.1).The motor stop for torque is not enough.then ride the bike forward in generate power mode, gMotorVars.Speed_krpm is alawys positive.
If set gMotorVars.IqRef_A _IQ(-0.1) to simulate ascent road, then ride bike make PMSM motor forward again,gMotorVars.Speed_krpm vary from -0.30 to +0.45(-300rpm to 450rpm),and gMotorVars.Torque_Nm vary between positive and negative also.
Why the estimated speed varies between positive and negative when rotor always forward?