Part Number: TMS320F28035-EP
Other Parts Discussed in Thread: TMS320F28035
Tool/software: Code Composer Studio
I am using TMS320F28035 microcontroller for ADC, GPIO and UART Application using C28.
In this application, i need to receive 20 Bytes of Data as command packet and send the status of ADCs and GPIOs on UART.
I tried using polling mode, which receives only last 4 bytes of data in buffer and rest all is getting discarded.
In case of interrupt mode data is received properly but other parts program in while(1) loop in not executing.
1) I would like to understand, which would be better approach to handle this 20 bytes of data(Interrupt or polling).
2) Kindly suggest the solution for the above issue of polling mode and interrupt mode.
Regards Ajay