Part Number: TMS320F280041C
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
Greetings! I`ve reached is04_signal_chain_test. My motor is running correctly on the hardware test. But on test 4 it doesn`t run at all. I`m not sure what values should I set to speedRef_krpm,IdSet_A and IqSet_A. Now the controller is generating a PWM with 50% duty cycle. I`ve tried example 5, but there the motor made just a few rotations and stoped without reaching the point where I have to lock the rotor(I`m using ACIM). Do you have any idea what is wrong?
Thanks!