Part Number: TMS320F28374D
HI everybody
According to the datasheet,t the minimum time of Sample window duration is 75ns. I could find example project that uses this configuration (oversampled) which is adc_soc_continuous_cpu01. The example project uses only one channel to use SOC continuously.
However, in my code, I used multiple channels and tried to use SOC continuously. I had to give at least 150ns of sample window duration (ACQPS) to get the right ADC reading. why ?
is The min time 75ns can be only applied to a single ADC channel for continuous SOC (oversampled)?
Best regards
Carlo